Part Number: TX7332
I have two TX7332 connected to an AFE, sharing channels.
I want to pulse on one TX7332, but switch off the TR_Enable for the duration of the acquisition.
Similarly on the 2nd TX7332, I want to switch on the TR_Enable for the duration.
What is the correct way to switch off the TR_Enable?
For the transmitting channel, do I extend the Period to be off for the whole acquisition duration?
This appears to be very contrived......
For the receiving channel, this is not a problem: I set up the Period registers as per normal, with level registers at 0V.
If this is incorrect, please let me know.