This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131E08: Readings multiples of ten

Part Number: ADS131E08


I just realized my ADC redings are multiples of ten, I have 4vref with 16ksps G=1. Do u know the reason?

-103090 -135290 -139770 -120230 -215080 -260580 -275800 -316370 80970 -240960
-103000 -134660 -140190 -121890 -214070 -260570 -274090 -317660 78670 -245910
-102790 -133920 -140960 -123220 -212930 -260420 -272430 -319020 76340 -251100
-102520 -133400 -141570 -124660 -211810 -260150 -270800 -320190 73940 -255970
-102380 -132770 -142180 -126010 -210580 -260040 -268800 -321230 71350 -261000
-102270 -132230 -142840 -127360 -209480 -259610 -267000 -322220 68690 -265690
-102090 -131390 -143470 -128880 -208240 -259220 -265160 -322920 65860 -270500
-101920 -130800 -144150 -130260 -207090 -258870 -262930 -323750 63320 -275360
  • Hi Alberto S. G.

    Is it possible you are reading the data incorrectly, or converting incorrectly?

    Can you post the actual raw hex data from the ADC instead of the converted values?

    Would the data be correct on a per channel basis if you scaled each value by 10? For example, does -10309 correspond to the correct voltage you expect to read on that channel?

    -Bryan

  • We have reviewed the ADC_OUT with an oscilloscpote and the frame sent by the ADCs looks multiple of ten too.

    This screenshot show the treated frame we share 

    It´s backwards: 

    0x00c00001 (header ADC1)

    0x00c00800 (header ADC2)

    0x00c00000 (header ADC3)

    0x00000578 (ch1)

    0xfffffb6e(ch2)

    0xfffffc4a(ch3)

    ....

    We convert the 24bits complement´s two to 32 bits before of sending.

    We have an external CLK of 1.88MHz instead of 2.048 in order to get 14.4ksps instead of 16ksps (DR CONFIG1=010).

    Vsupply + - 2V5

    Vref 4V

  • Hi Alberto S. G.

    0x00c00001 (header ADC1)

    0x00c00800 (header ADC2)

    0x00c00000 (header ADC3)

    I don't understand what "(header ADC1)" means, can you explain?

    I asked some questions in my previous post, can you help answer them:

    Can you post the actual raw hex data from the ADC instead of the converted values?

    I'm looking for just the raw data, not anything you have sign extended or manipulated in any way. You can use a logic analyzer to pull the data directly from the ADC DOUT pin.

    Would the data be correct on a per channel basis if you scaled each value by 10? For example, does -10309 correspond to the correct voltage you expect to read on that channel?

    It is helpful to know what you expect to read versus what you are actually reading. Or, if you apply a 1V signal to the ADC and take 1000 samples, what values do you get?

    -Bryan

  • Sorry Brian,

    Yes, I think the value is the expected, but we are losing accuracy.

    by example:

    -3V (Vref 4)->  (-6291456 expected) --> 6291450 (read value ignoring the noise)

    1V (Vref 4)->  (2097152 expected) --> 2097150 (read value ignoring the noise)

    I have a testing SW that gets a 1sec capture and the noise surround 0.1 mV but it could be due to my circuit. No worried for now :)

    The point that I can´t understand and I would like to discover is why the value always is finishing in 0.  

    I ask my partners about the raw data, but the couldn´t provide me it. They just read de ADC_OUT pin with an ocilloscope and confirm me that the read values finished with 0. I will use a logic analyzer and try to read DOUT.

     The header that I meant is the first register we ask to the ADC_DOUT with the status registers.

  • HI Brian!

    We just realized that if we choose a 8ksps data rate instead of our 16ksps that we need. The issue is solved.

     COuld it be a ENOB problem? Does the ADC replace noise with zeros?

  • Hi Alberto S. G.

    Thanks for answering my questions, and clarifying your results.

    The ADC should not artificially change the output data depending on the data rate, unless you are operating at 32kSPS or greater where the ADC only outputs 16 bits of data. In fact, it really should be the opposite, where the lower bits are toggling at higher data rates because there is noise, whereas at lower data rates that have less noise those last bits could be stable

    I should also point out that being off by a few codes is actually really good. You can see from Table 2 that the ADS131E08 is not a 24-bit noise-free ADC, in fact the best effective resolution (ENOB) you should expect is around 20 bits at the lowest data rate. At 16 kSPS you should expect around 17 bits of resolution, so only being off by a few codes is way better than expected. I still am not sure why that last bit was not toggling at 16 kSPS, but is toggling at 8kSPS. You are definitely operating at 16 kSPS, not 32 kSPS? And you have all channels enabled?

    -Bryan

  • Yes, we have DR 16ksps, this screenshot show the DRDY edge every 62us.

    According with our ENOB, 17.33bits (Vref=4 DR=16ksps) we should have 24.27uVnoise and the info I´m losing corresponds to 47.6nV.

    The point we wanted was understand it, in order to avoid strange behaviours and improve the functionality...

  • Hi Alberto S. G.

    I don't think anything is wrong here, as you don't appear to have a stuck bit since it is toggling when the data rate = 8 kSPS. But I agree it does seem like non-random behavior for the last bit to always be a 0

    Can you read back the data multiple times between DRDY periods to see if it is the same every time? Note the requirements stated in the datasheet for multiple read back, which I copied below

    Can you also take 1000 samples of data at 16 kSPS and 8 kSPS with the same input voltage applied (or shorted inputs), and send that data to me so I can review. Again, it would be helpful to see the raw ADC data, not data you have manipulated in code. You can also provide the data for all 8 channels

    -Bryan

  • Hello Brian,

    I am attaching both captures, with 8ksps and 16ksps. We have 12 channels, and in this case we configured the channel 4 (fourth column) with MVDD as datashhet said, in ch4 MUX[2:0] = 011 means MVDD/4 in our case, 3.3/4.

    The data is signed decimal with 4Vref.

    analog_info_8KHz.txtanalog_info_16KHz.txt

    We need modify our code to get more than one capture in the same DRDY. I am sharing with you the captures when we get it.

    THank you a lot !!

  • Hi Alberto S. G.

    I'm having a hard time believing that the ADC is doing this. This is not just LSB = 0, which could be possible, but it is the entire 24 bit frame always adding up to a multiple of 10 in decimal.

    Is it possible that there is a timing issue as you increase the clock rate, which is why it works at 8kSPS and not at 16kSPS? Does it work at the lower data rates? Again, seeing the actual data on a logic analyzer is the only way to tell what's going on. The data you sent it not very valuable because there's always a chance that the conversion process messed something up

    -Bryan

  • Hi Brian, We got a few frames of the 16ksps raw data of DOUT. We have no analyzer so it was a bit hard. But I hope it's worth it Slight smile

    As you can see, every channel measure ends in zero. it seems that is not a conversion issue. He have no faults in the status word and the GPIO bit up is an active low reset...

    C000010003C0B05550FFF272FDC704FFFABAFFFAF6FFFBDCFFFBA0
    C000010003B6B05514FFF1B4FDC6E6FFFACEFFFAECFFFB1EFFFBB4
    C0000100037AB055A0FFF1E6FDC736FFFAB0FFFAF6FFFAECFFFBA0
    C00001000320B055AAFFF0ECFDC75EFFFB1EFFFAE2FFFB1EFFFBA0
    C00001000352B05582FFF09CFDC7B8FFFAC4FFFB00FFFB5AFFFBBE

    Let us know if these few plots can help you to understand what is happening...

    Thank you!!

  • Hi Alberto S. G.,

    Let me look into this more and get back to you tomorrow

    -Bryan

  • Hi Alberto S. G.,

    Apologies, I could not look into this today, I will try to have something for you by the end of the day on Monday

    Thanks for your patience

    -Bryan

  • Hi Alberto S. G.,

    I reached out to our design team to see if they have any feedback on this issue. Again, there doesn't seem to be anything wrong as the data is well within the limits you would expect sampling at 16 kSPS.

    On how many devices have you seen this behavior? Just 1? Have you tried replacing the device with a new one to see if the behavior follows the board or the device?

    -Bryan

  • Thank you Bryan.

    Every prototype has 3 ADCs sampling simustaneously and they have always the same behaviour at 16ksps.
    So you mean it is ok to have steps of 10 in the measures? this is the point we wanted to know, discard a config problem.

    Thank you Bryan! You've been very helpul :-)

  • Hi Alberto S. G.,

    I was able to confirm with my EVM that this is in fact how the ADC behaves. So there is no issue with what you are seeing, this is the intended device behavior at 16 kSPS. The "rounding" will not cause any issues with your measurements, because the noise level is >10 codes anyway.

    -Bryan