Other Parts Discussed in Thread: TSW1418EVM, ADC3683, TSWDC155EVM
I am using the TSW1418EVM with the ADC3683EVM, and have discovered that I need two RFsignal generators (65MHz and 292.5MHz) to supply both Sampling clock on J4 of the ADC3683EVM, and the DCLKIN clockon J9 of the EVM... And maybe ideally another RF signal source to test its performance!?!
I don't have access to two RF signal generators at the moment (forget three!)...
Also, if I wanted to use this ADC in my product designs, I want to be using a PCB-based clock source!
I note from the very good support documents for the ADC3683EVM that there is a signal input connection alternative for DCLKIN_FPGA_P and DCLKIN_FPGA_N from the interface with the TSW1418EVM, and the option of FPGA_CLK or FPGA_REF_CLK as alternative onboard clock sources, again from the TSW1418EVM interface
There is also provision for a four-pin clock source package (Y1) for the sampling clock, but no alternative input other than the J4 interface for the LVDS clock (so I am hoping that the TSW1418EVM can supply that clock...?
Any comment on using these alternative clock sources?
Perhaps they are not implemented on the TSW1418EVM, or not properly debugged and therefore not advisable to use?
Any practical information appreciated.
I am perfectly capable of soldering and desoldering 0 ohm links, or other components to mould this ADC3683EVM PCBA to my needs if that is what I need to do, but it would be useful to know if that is not advisable.
I can find no blogs or accounts online of someone using these kits to evaluate the ADC3683, but would be very willing to construct one myself if I can get this going!