Other Parts Discussed in Thread: DAC38RF82
Hello,
I am evaluating DAC38RF82 with the evaluation board and the pattern generator.
A 100 MHz / +6dBm signal is fed to the input of the LMK (J4 connector).
With the following configuration (only one DAC), all is right, a correct spectrum is present at the output of the DAC.
When the configuration is changed to 8 lanes (instead of 4 lanes), the Serdes Lane Rate is twice lower, there is no other configuration change than the HSDCPRO file (suffix 821 instead of 421) :
On the HSDCPRO GUI, when loading the right ini file (suffix : 821), the following pop-up message appears:
And after resetting DAC JESD Core (DAC GUI), it is not possible to have a spectrum at the DAC output (no signal at all).
I suppose that this is due to the JESD reference clock (to TSW14J57) which has to be set to 200 MHz (instead of 100 MHz).
What is wrong with this configuration ?