Part Number: TX75E16
Other Parts Discussed in Thread: TX7516
Hello,
I am looking for technical support regarding Ultra Sound Pulser.
we're interesting in driving 16 capacitive elements (MEMS) - at the same time.
When the capacitance of each element is: 50pF
The frequency: 400 KHz
And the output voltage (on each element): 50Vp-p, they will be happy if it is possible to reach 80Vp-p.
Note: there is no need for Rx function
Summery table:
|
Parameter |
Min |
Nice to have |
|
Capacitance load per 8 output channels (pF) |
250 |
400 |
|
Voltage |
50 |
80 |
|
Freq. kHz |
400 |
400 |
Q: Is it possible for the package not to reach the limit of power dissipation on the packaging, and maximum heat at the semiconductor junction?