Other Parts Discussed in Thread: TVP5147, TVP5147M1
Are there any special hardware considerations when connecting two TVP5147's on the same bus? It looks like from the datasheet that once they are out of reset, only the INTREQ signal is driven.
If the INTREQ is not used, is it safe to connect other pins on the same bus without any switches or multiplexors?
Jeff