Part Number: AFE5401-Q1
Hi. I have questions about 100 MSPS Data Processing.
I'm curious about how AFE5401 processes data when it has maximum sampling rate.
As far as I know, if it is 25 MSPS per Channel, the period of output data is 100 MHz.
Since AFE5401 outputs data in parallel, it is necessary to combine the data into one value.
A very high DSP clock is required for me to represent a parallel signal output at a period of 100 MHz as a single value and then store it in an array one after another.
Is there a DSP of TI that I can use in this case or is there another way I didn't think of?
Ultimately, what I want to know is that when the sampling rate of AFE5401 is maximum, I want to know how the DSP of TI handles it.
Thank you.