Part Number: ADS5294
Are all of the digital inputs
PD
RESET
SCLK
CSZ
SDATA
SYNC
compatible with 2.5 V logic level signals (i.e., with outputs from FPGA pins configured as LVCMOS25)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yes , It should work as it is grater than the VIH required from device .