I'm using the ADS1262 with a custom pcb. I can read and write config registers perfectly fine but when I do a RDATA command I always get back 01111111 11111111 11111111 11111111 as the response no matter what.
Is there a common cause for this? All settings are set to default aside from turning off the checksum and status bytes for simplicity. I followed the flow chart in the datasheet as best I could but I get this result no matter what. Doubling the size of the transmission data buffer repeats this output. Is it some king of shifting error or am I missing a setting? Any insight is much appreciated.