Other Parts Discussed in Thread: LMK00334,
Hello team,
Can I use HCSL signal as clock input (CLKP, CLKM)?
Best Regards,
Kei Kuwahara
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yes, as long as it's AC-coupled and the differential swing is at least 1Vpp then it will work.
Hello Geoff-san,
I have additional question to this.
My customer is considering to use LMK00334 to input HCSL clock signal.
From the datasheet of LMK00334, HCSL output clock looks like only 0.8Vpp.

Would it be possible clock ADC3562 with only 0.8Vpp?
Best Regards,
Kei Kuwahara
Kuwahara-san,
800mV is single-ended so is 800mVp (peak). Differential of that is 1.6Vpp (peak-to-peak) so it will work.
Regards,
Geoff
Hi Geoff-san,
Thank you!
I forgot it is differential signal.
Best Regards,
Kei Kuwahara