Part Number: ADS1299-4
Other Parts Discussed in Thread: ADS1292R, ADS1298R
Hello guys,
One of my customers is considering using ADS1299-4 for their new products.
At this moment, they have the following question.
Could you please give me your reply?
Q.
ADS1299-4 datasheet says that Digital power supply is 1,8V(Min), 1.8V(Nom), 3.6V(Max).
The customer apply 1.8V to ADS1299-4 as the digital power supply because another logic circuits uses 1.8V.
This voltage may be lower a little than 1.8V depend on production variation.
If the digital power supply voltage is just a little below 1.8V, will ADS1299-4 digital operation stop?
Also why are the nominal and the minimum voltage same?
Your reply would be much appreciated.
Best regards,
Kazuya.