Part Number: AFE58JD32
I am using the LVDS mode of AFE58JD32 for data acquisition. I can collect the correct ramp data, sync data and deskew data. There is a problem when collecting ADC data.
Now I have two questions:
1.When I collect ADC data after turning off the LNA and LPF, there will be a lot of glitches (figure1)in the data, but there are no glitches(figure 2) in the ramp data.

figure 1

figure 2
2.When I enable LNA and LPF and connect the waveform generator to the signal input section, even if the waveform generator does not output a signal, the ADC output will be full scale (figure 3).

figure 3
The following are some configurations about ADC
1.The ADC_CLK is 10MHz(5Msps/ch);
2.The data interface is LVDS x1 rate;
3.The Digital processoing module and the Demodulator are bypassed;