This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12QJ1600: ADC12QJ1600

Part Number: ADC12QJ1600
Other Parts Discussed in Thread: LMH32401

Hello,

I design a new Lidar using the TIA LMH32401 connected to the ADC12QJ1600. (see schematic).

My question is : do I need to add input protection to the ADC inputs and if yes, do you have any recommendation.

- The max positive output of the LMH32401 is 2.9V (data sheet).

- The max input voltage of the ADC is 2.1V.

Schematic:

Regards,

Giora