Part Number: ADS1278
HI team ,
I am Working in the project of data acquisition system so we need 8 channel input in this case we choose the ADS1278. To configer the ADS1278 through the SPI protocol,
we are configer the configeration through the I/O pins
ADS1278 Input Pin -TEST pin[0:1] //this pins are set to LOW Because we use Normal Mode.
ADS1278 Input Pin -FORMAT pin[0:2] // this pins are set to LOW Because we use SPI TDM Dynamic formate.
ADS1278 Input Pin -MODE pin[0:1] //this pins are set to LOW Because we use High-Speed Mode.
ADS1278 Input Pin -POWER DOWN pin[0:8] //this pins are set to HIGH Because we use 8 Channel of input.
ADS1278 Input Pin -CLKDIV pin 1 //this pins are set to HIGH Because we need Higher sample per Second.
ADS1278 Input Pin -CHIP SELECT/SYNC pin 1 //this pins are set to HIGH OR LOW(Based on the condition).
ADS1278 Output Pin -DRDY pin 1 //Read the pin.
FCLK=25MHz
SCLK=25MHz
After the configeration
First CHIP SELECT/SYNC pin put low
After monitering the DRDY pin //When the pin is Low ....Move the next condition.
In spi write 24 Bytes data=0 will send / Also 24 Bytes of SCLK will also send.
But SPI Read function there is no data is recived
CHIP SELECT/SYNC pin put HIGH...... In this time DRDY pin is gose to High
HOW to Retrieve the data....?
Please give me a reference code.
Thanks and Regards,
Aravind.SR