This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC081C021: ADC081C021CIMM

Part Number: ADC081C021


Hi,

I just wanted to confirm that the operating temperature range of the VSSOP version of the ADC = ADC081C021CIMM

is compatible with the operating range -40°C / +105°C ?

In the datasheet of the ADC081C021, the temperature range is missing on the VSSOP package. As for the TI website. The webpage mentions the temperature range for all the device versions, except for the VSSOP package.

Thanks for you precisions.

Best regards.