Part Number: AFE4404
I have a special test mode that is need. It requires that all three LEDs be on at the same time for most all of the Repetition Interval.
The "normal" operational settings are for 100Hz at 1% duty cycle, with typical sequential sampling and conversion.
For purposes of the test routine I would like to just change the 3 led on intervals to be the same.
Normal values:
LED1 802, 1201
LED2 0, 399
LED3 401, 800
PDN 5475, 39199
Proposed for test mode:
LED1 0, 38950
LE21 0, 38950
LE31 0, 38950
PDN 39000, 39199
Is this a "valid" timing from a hardware functional point of view. (If the led drive current source is multiplexed between the different LEDs then of course this would not work...)
Thoughts/ comments?