Part Number: DAC11001B
There is a section in the DAC11001B datasheet that states:
7.5.3.2 Asynchronous Update In asynchronous mode (LDACMODE = 0), data are updated with the rising edge of the SYNC (when daisy-chain mode is enabled, DSDO = 0), or at the 32nd falling edge of SCLK (When daisy-chain mode is disabled, DSDO = 1). For asynchronous updates, the LDAC pin is not required, and must be connected to 0 V permanently.
If instead, the LDAC pin is connected to +3.3v permanently, how will this affect performance? We are seeing significant sinusoidal temperature sensitivity across -40 to +80 degC while using this device.