Other Parts Discussed in Thread: ADS8201, ADS1115
Hi all,
I put this issue in other topic, but finally i see that topic was solved. Sorry about that.
In any case, I trying to implement a driver for ADS8201, I have some questions about protocol between ADC and microcontroller.
Datasheet don’t show SPI mode (00, 01, 10 or 11), What SPI mode use ADS8201?
I suppose that reset pin is always to high level if we want to operate in normal mode, if we want reset IC we only have to put reset pin to low level, ¿no?.
What is max. and min. baud rate of SPI?, I’m using by default 12MHz but I’m not sure if this baud rate work with this IC.
Have you any test to verify communication between microcontroller and ADS8201? In this case write register 0x08 with 0x00 (idle mode), then write resgister 0x04 with 0x00 (channel 0) and then try to read register 0x04 to see if after write work, but I receive noise and other times I receive only 0x00. You can see in the picture below.

I’m intersting in “manual-trigger, mode 2”, if you have some example to share with us it will be great for me.
I have some noise in SPI pins, do you recommend me put pull up resistor or serial resistor to prevent reflections?
Thanks for all.