This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In order to build a 3600W inverter from the texas TIDM-HV-1PH-DCAC demo board, we've modified some parameters, including the bridge topology, which now has two filter chokes, as on the other TIDM-SOLAR-ONEPHINV demo board.
We also changed the AMC1304M25DWs for AMC3336s, which were better suited to our application.
I'll need your help to validate the AMC3336 in this mode of operation:
Does the 4M resistance on one side imply an imbalance in the measurement that could upset the result? All the more so since transistors cause disturbances on both LINE and NEUTRAL.