This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS9219: Register setting for only using 1 device

Part Number: ADS9219

Hello team,

My customer only use single ADS9219, so they don't do daisy chain connection.

I wonder what is the difference between the settings below:

Setting 1.

Set Register 00h to Legacy SPI mode.

Setting 2.

Set Register 00h to Daisy-chain mode (Default)
And set Register 01h to 1 ADC (Default)

Customer is confused because default setting for Register 00h is Daisy-chain mode.
If customer is only using single ADS9219, then which setting is more suitable?

Best Regards,
Kei Kuwahara