Part Number: ADS1282EVM-PDK
Other Parts Discussed in Thread: ADCPRO, ADS1282, MSP-EXP430FR5969
Hello,
I had a question about the ADS1282 chip as well as the ADCPRO software. My current configuration is: PGA = 1. Ext. Vref = 1.25V, and my input range I'm currently operating under is from 0V to 1.25V. I have been using the following formula to convert the data I am getting from ADCPRO into voltage values: DATA*1/2*Vref / 2^30. And am assuming that whatever values I get from ADCPRO will be in millivolts. I am also using the default digital filter that is preselected on ADCPRO (Sinc + LPF Filter Blocks). I am also using a data rate of 250 SPS and operating this board in unipolar mode. The current problem I am having is that my input data is not quite lining up with what we're getting with out output data.

As you can see not even a differential input of zero outputs zero so I am wondering why that is. Another thing, I am using this chip for the project and currently using the ADS1282EVM-PDK board for prototyping. Because we are trying to use our own components with this chip we have decided to take off some components on the eval board. The main components we took out are the Op-Amps as well as the diodes:

So our external voltage reference as well as our input voltages will go directly into the ADS1282 without having to go through any Op-Amps or diodes that could manipulate the values being inputted. I would also like to know if there is a easy way to convert the output data values from the ADCPRO into the input voltages that were inputted into AINP & AINN.
Best,
Karam