Part Number: AFE11612-SEP
Other Parts Discussed in Thread: ADC128S102-SEP, DAC5675A-SP,
While analyzing the IC datasheet and comparing it with the other ADCs and DACs available in the TI product selector list, some queries were raised.
Kindly provide a solution for the same.
Application: For controlling and monitoring the signal of a power processing unit for a Hall Effect Thruster.
Clarification:
- Is the accuracy of the IC dependent on the temperature, since the IC has an inbuilt temperature sensor, or is it a feature?
- Whether there is high power dissipation and thus higher temperature rise?
- Even though the functionality is more for AFE11612-SEP compared to the ADC and DAC such as ADC128S102-SEP, ADC128S102QML-SEP, DAC5675A-SP, etc., why is there a significant difference in the cost aspect? Could you please explain it.