Part Number: ADC3682
the ADC3682 datasheets recommends ambient Temperatures between -40°C and 105°C.
What happens when we use the part at -54°C, is there only loss in performance or will th part be destroyed?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADC3682
the ADC3682 datasheets recommends ambient Temperatures between -40°C and 105°C.
What happens when we use the part at -54°C, is there only loss in performance or will th part be destroyed?
Hi Hans,
At first it will be a loss of performance but long term reliability is unknown outside of the recommended operating temps.
Regards,
Geoff