Other Parts Discussed in Thread: ADS1261, , ISOW7741, ISO7741
Hello,
I need to use a galvanic isolator with the ADS124S08 or ADS1261, for both power and SPI.
The ISOW7741 seems to be a really good option.
I need to use the EN_IO1 to put the SDO/MISO line in high impedance.
I am not absolutely sure that the disabled states for the SDI/MOSI and SCLK would be what the ADC would expect.
Would it be possible to combine the EN_IO1 and CS?
Do I need to use the ISOW-7741-F instead?
I would greatly appreciate your comments.
Regards,
Christian