The datasheet page 10 says that: All digital inputs support 1.8V and 3.3V CMOS logic levels.
Can I use LVCMOS 2.5 logic? I would like to eliminate the use of a superfluous level translator.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The datasheet page 10 says that: All digital inputs support 1.8V and 3.3V CMOS logic levels.
Can I use LVCMOS 2.5 logic? I would like to eliminate the use of a superfluous level translator.
Hi,
The datasheet table shows the minimum VIH for the device to interpret a "high" and the maximum VIL that is required for the device to interpret a "low". If the VIH/VIL meet these requirements then the part will operate as described in the datasheet.

Regards,
Geoff