Part Number: ADS52J65
Other Parts Discussed in Thread: LMH6553,
Hi,
I am in the process of developing an ADC PCB. I intend to use the ADS52J65 ADC, for which I have already performed initial tests with your evaluation board to verify the basic functions.
At this stage of the project I am looking for suitable fully differential operational amplifiers (FDA) that can drive the ADC effectively. A particular requirement is that the op amp selected includes a clamping circuit to protect the ADC from overvoltage.
While searching for possible options, I came across the LMH6553, which seems to meet our specifications. However, when reviewing the compatibility table in the datasheet, I noticed that the ADC we wanted, ADS52J65EVM, was not listed. It is worth noting that our application requires a signal bandwidth of 60 MHz.
I would be very grateful for any advice or recommendations on suitable op amps for this application.
Kind regards,
Alexander Schulz