This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8689: CONVST/CS and SCLK are LOW when RST low-to-high transition?

Part Number: ADS8689


Hi Experts,

Good day.

Paragraph 7.4.2.1. RESET state

"In order to exit any of the RESET states, the RST pin must be pulled high with CONVST/CS and SCLK held low.
After a delay of tD_RST_POR or tD_RST_APP (see the Timing Requirements: Asynchronous Reset table), the device
enters ACQ state and the RVS pin goes high"

Does this mean that CONVST/CS and SCLK must be held low during the RST low-high transition, or does the ADS8689 leave the RESET state the at the earliest occasion when /RST high, /CS low and SCLK low applies concurrently?

Thank you for your assistance.

Regards,
Archie A.

  • Hi Archie,

    The top of the 7.4.2.1 section tells you that it is an asynchronous reset, so getting into the reset state is easy.  Once you release /RST, you can re-configure the part.  SCLK is low by default so if you want to resume conversions, SCLK should be low with CONVST high.