This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ5200RFEVM:  ADC12DJ5200RFEVM:how to use the software of ADC12DJ5200RFEVM correctly

Part Number: ADC12DJ5200RFEVM
Other Parts Discussed in Thread: TSW14J57EVM, , LMK04828

To quickly verify whether the ADC12DJ5200RFEVM and TSW14J57EVM are working correctly using JMODE1 and to check the performance parameters, I selected the External Clocking Option with the following settings:

  • REFCLK (J17): 260 MHz
  • LMK04828 SYSREF: 32.5 MHz
  • REFCLK (J10): 5200 MHz

I performed the following steps but encountered some issues.

1.

Select JMODE1 and complete the firmware programming.

Set the ADC output data rate to 10.4G.

2.

I have installed Python version 2.7, but every time I open the ADC GUI, it prompts for reinstallation and displays a dialog box. Does this have any impact? Additionally, when I click on "Script" to view the script, it appears as gibberish. 

When I try to modify the External Fs Selection, the above-mentioned dialog box also appears, and I cannot change the value.

I selected JMODE1 and then clicked "Program Clocks and ADC."

I clicked "Update Temperatures" to read the ADC Temp and LMP95233 Local Temp. Are the values normal?

I am unable to modify the FPGA Reference Clock to 260 MHz, Sampling Frequency to 5200 MHz, and SERDES Rate to 10400 MHz. How can I make these changes?

3.

Is the status on this interface normal? Are there any parameters that need to be set?

4.

Is the status on this interface normal? Are there any parameters that need to be set?

5.

Is the status on this interface normal? Are there any parameters that need to be set?

6.

I need to configure the parameters of the 04828. How do I set them according to my requirements(FPGA Reference Clock=260MHz,Sampling Frequency = 5200MHz,SERDES Rate = 10400MHz)?

7.

The D4 LED on the TSW14J57EVM board is not lit, while the D3 LED is lit.

When executing these steps, I encountered the mentioned issues. My computer runs on Windows 10 64-bit.Could the issues be caused by the software being 32-bit? Additionally, how should the LMK04828 be configured, and is there a quick setup guide available? Thirdly, are there any specific requirements for configuring SYSREF?