Hello,
I have go through the ADS5281 datasheet, As datasheet mentioned the two technique for the single ended input to differential with respect to the input infrequency,
- one for low input frequency
- second for hign frequeny.
Que1: So my question is that, What will be the Low frequecy and high frequency range?
We have two options as we have 16 Analog input signals,
Option1 :- We will use Two ADS5281
Option 2: We need the IC with 16 channel Analog Input.
Que2: Can you please suggest the 16 channel Analog Input IC ?
Regards,
Alpesh