This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF1208-AFE7950EVM: TRF1208-AFE7950-EVM Evaluation Module - Configuration

Part Number: TRF1208-AFE7950EVM
Other Parts Discussed in Thread: TSW14J57EVM, AFE7950

We are developing a direct conversion system for X-Band Radar and, for this purpose, we are considering using the TRF1208-AFE7950EVM + TSW14J57EVM set as an initial proof of concept. I would like to know if it is possible to generate and convert the signal in the X-band, specifically at 10GHz, using the DAC and ADC. What would be the configuration (JESDMode, NCO, etc.) to meet this requirement?
Additionally, I couldn't find information about the JESD mode of the AFE7950 component datasheet. Could you share the possible modes of this component?

  • Hi Luiz,

    In the AFE79xx GUI we have example scripts that are already configured to operate in X-band, 9.5GHz. These scripts can be updated such that the NCO frequencies are set to 10GHz. Please download the latest version of our GUI and the examples scripts will be under the AFE7950 folder. 

    If you can fill in the table below we can point out the example script that you be used as a starting point, or customize a script for you.

    Regards,

    David Chaparro