Part Number: ADC12DL3200
Other Parts Discussed in Thread: LMH3401, LMH5401
Hi,
I am using ADC12DL3200 part in my custom design. ADC gets input signal (of bandwidth DC to 750MHz) from a demodulator, so I can only use DC couple interface. Demodulator output has a bias voltage of 0.9V, but the input common-mode voltage of ADC12DL3200 is 0V. So I am using resistive translation circuit as given below

Please confirm if the values given are proper. (Considering Current of 10mA).
Thanks in advance