Other Parts Discussed in Thread: DAC7311, DXP
Tool/software:
Where to download the drivers of MMB0 for windows 10 or above ?
I used the MMB0 board with DAC7311 EVM,the evm had pluged into MMB0,and the DC input for the MMB0 is +5V, the MMB0 connected my PC with the USB cable , but windows can't recognized MMB0 ,MMB0's name in the PC is "unknown device", see the picture below :

I had installed the Labview 2024 , but when I run the DXP software from Ti ,there was a notication like the picture below :