This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW14J57EVM: TSW14J57revE_BRAM_RxOnly_16L_FIRMWARE Download

Part Number: TSW14J57EVM

Tool/software:

Hello, is there a BRAM firmware source file for the TSW14J57? I am looking to download the source files for TSW14J57revE_BRAM_RxOnly_16L_FIRMWARE or similar. Thank you

  • Hi Ryan,

    Unfortunately, the FPGA design used on the TSW14J57EVM was developed through a third party and is available only as a bitfile (source code cannot be shared). In addition, it contains a Xilinx JESD IP, which needs to be licensed directly from Xilinx. If you are looking to create a JESD based FPGA design and your target is a Xilinx FPGA, kindly requisition the TI JESD IP from the following link:

    https://www.ti.com/tool/TI-JESD204-IP

    The JESD IP archive contains a number of generic reference designs that you can use as a starting point and then customize for your specific link parameters.

    Regards,

    Ameet