Tool/software:
Hi, I am currently working with ADS5560 by using internal reference.Firstly, I set full scale input range with 0 dB. It means that 3.56Vpp voltage can be readable from ADC by using 1.5V VCM reference like 1.5 +-1.78V. However, when I set register 68 with 1000 I see that I can only measure signals with ranges 2Vpp between 1.5 +-1V. Also It doesn't provide 65536 output code range.