Part Number: ADS8320
Tool/software:
Hi
I am sorry for this petty question but i did not find a formal answer in ADS8320 documentation : is DOUT output type format tri-state or CMOS ?
Thanks for help
Olivier
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS8320
Tool/software:
Hi
I am sorry for this petty question but i did not find a formal answer in ADS8320 documentation : is DOUT output type format tri-state or CMOS ?
Thanks for help
Olivier
Hi Oliver,
Welcome to our e2e forum! The ADS8320 Dout goes tri-state after time 'tDIS' as noted in Table 1 (pg. 14) and Figure 34 (pg. 25) of the datasheet.
Hi Tom,
I noted that but there is no mention of pullup or output sink current anywhere in the datasheet, neither in table or figure, and CMOS output logic levels are provided in table §6.5 in such a way that DOUT is not open drain. In my design DOUT is acquired through a 74LVC541 buffer so should i add a pull-up on buffer input or not ?
Regards
Olivier
Hi Oliver,
You do not need a pull-up on the DOUT line for proper operation of the ADS8320. Adding one would not hurt anything, so the decision in the end is up to you.