Part Number: ADC084S101
Other Parts Discussed in Thread: ADC082S101
Tool/software:
I conisder to use this component for AC signal sampling. I want to make sure befire using it. Therefore, I really appreciate your feecback to find a proper component.
The input AC input signal varying from 0 to 5V and 0 to 250 kHz which I want to sample. The microcontroller supports SPI with 8MHz or max 32 MHz clock frequency.
I wonder whether to achieve continuous sampling of an AC signal from 0 to 250 kHz (each channel) by using the SPI with 8 or 32MHz through ADC084S101? I will use all 4 channels for sampling at the same time.
Otherwise, would you have any other prodcut suggestion for me?
Thank you in advance