Part Number: DAC7716
Other Parts Discussed in Thread: DCP020515D, , ADS8883, OPA4990, DAC8234, DAC8734, PGA855
Tool/software:
Hello,
I am using two DAC7716 on our board and they are being powered by a DCP020515D part. Through testing at around 75C we found that the DCP020515D would go into what looks like thermal shutdown because the output rails of the part are rock solid +/-15V until all of a sudden at around 75C they have huge amount of ripple at around 150KHz approx and I take that to mean that the part is going in/out of thermal shutdown?.
I removed the DCP020515D and used an external power supply instead. As the temperature rose, I saw the negative supply current rise from 50mA to about 200mA by the time 85C was reached. This indicated to me that the issue is not with the DCP020515D shutting down but instead there is a load problem.
Setting the board on the bench and continuing to use the external power supply, and now this time rather than heating up the entire board I used a reflow pen at its lowest setting (100C) and kept the pen around 0.5-1 inch away from parts and move it around the board looking to see which semiconductors would cause an increase in negative supply current. Moving the pen over the DAC7716 would increase the current by 50mA at the elevated temperature
Normal negative supply current is around 40-50mA at room temperature. At around -30C the negative supply current is around 30-40mA..
Any suggestions?