Other Parts Discussed in Thread: LMK04821
Tool/software:
Hi,
a few years ago we build a data acquisition board with 4 x ADC31JB68RTA25 connected to an Xilinx Artix.
The ADCs are clocked with 400 MHz. The Xilinx FPGA filters the data and sends them to a PC over Ethernet.
We got the board working, with the help from an TI engineer, who told us to set a undocumented bit
in an register.
We now build more boards, however, as that part is not available anymore we used 4 x ADC31JB68RTAT.
The new boards seem to sample data, however the received data on the PC look different, as if the sample
rate is not the same.
We suspect there might be a difference between the ...RTA25 and the ...RTAT version. Switching the ADC into
testmode to generate a ramp between 0x000 to 0xffff works. I cannot see any notes int the datasheet, regarding
the RTA25 and RTAT version. What is the difference between the two versions?
Cheers,
Ralf