Part Number: DAC8775
Other Parts Discussed in Thread: DAC8760,
Tool/software:
Hi TI Team.
When trying to detect open circuit in current mode output, it appears that the ALARMn output is asserted only when the current setting is greater than some 18mA. At currents below 18mA and at any negative current setting, an open circuit is not detected.
When setting the current at the 'right' setting, it will assert and de-assert the alarm output continuously. Setting the current output just below this point, then at first the ALARMn is not deasserted. Then after a while the ALARMn output starts asserting/de-asserting at smaller and smaller intervals.
Picture #1: Alarm output at 18mA, ALARMn asserts/de-asserts continuously.

Picture #3: Output current setting changed from 12.2mA to 18.1mA. At 12.2mA setting no open circuit is detected, causes the alarm output to finally assert through a lot of assert/de-assert cycles.

Can you elaborate on this, please.
looking forward to hear from you.
BR Henrik Buhl