Other Parts Discussed in Thread: LM27762,
Tool/software:
Hello everyone,
Recently, I have been using this ADC chip to collect voltage in a transimpedance amplification setup. However, I encountered an issue with excessive current during use. When the PCB is first powered on, the operating current is below 100mA. Within 1 to 2 minutes, it steadily rises to 600mA. Since I'm using the LM27762 power supply chip, when the current rises to 200mA, the negative voltage output starts to drop slowly from -2.5V to -2.2V, causing zero drift in the front-end amplifier.
Currently, I can communicate with the ADC via SPI normally when the current is stable, but the high current affects the power supply voltage, leading to measurement accuracy problems on the PCB. I tried removing some components to determine if other components were causing the issue, but it didn't help. Only when the ADC is removed does the current drop to around 10mA. My circuit is essentially consistent with the reference design in the datasheet. Below is the schematic of my PCB design. I hope you can help me identify the problem. Thank you.
In practice, I replaced the 1.8V digital power supply chip with a 3.3V chip to communicate properly with the FPGA.