Other Parts Discussed in Thread: ADS7861, ADS7863
Tool/software:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Linh,
Thank you for your question.
The ADS8361 does not have an ibis model, but its lower resolution version does (ADS7861), which can be used as an alternative.
Best regards,
Yolanda
Hello Linh,
I have to apologize, I made a mistake when looking for the ibis models, the device with the ibis model is ADS7863 not the ADS7861. I am sorry for the confusion on my part.
ADS7863 is similar to the ADS7861, but it has additional features so it is not a good ibis alternative for either the ADS8361 nor ADS7861. Meaning I cannot provide a suitable ibis model alternative for the ADS8361.
If having an ibis model is required and there is still an option to use a different device, there are some newer devices that are similar to the ADS8361 that do have ibis models, like the ADS8354 or the ADS8363.
Again, I am sorry for the confusion.
Best regards,
Yolanda