Tool/software:
Hello all,
I have few questions with respect to ads8634 interfacing.
1. Is driver is mandatory to interace the ads8634 with mater device via SPI ? ( master- jetson xavier nx)
2. For the AL_PD pin , In the 8th page of the datasheet it is metioned as below :
Digital input : low, asynchronous power-down.
The device features an internal, weak pull-up resistor from the AL_PD pin to DVDD. The
AL_PD pin can also be floated when programmed as a power-down input.
(The default condition for this pin is programmed as a power-down input pin.
Here i want to clarify , "if the AL_PD pin is floating ,then is will act as power down input pin and when it is configured as input pin then it will have a weak internal pull up " I wonder if my udnerstanding in this is correct.
Above in our case the pin is left floating. So i wonder here it will get a weak internal pullup or it will be in power down mode (default configuration). Becasue the data i am receiving is always "0" for any register .
Best Regards,