Other Parts Discussed in Thread: ADS5474, ADS54RF63, ADS5463, ADS5400
We ae considering the best way to sychronize several ADS5474 devices for simultaneous sampling at 400Msps. The ADCs feed an FPGA as whon in the attached document. One option is to use DDR signal DRY to clock in the DATA to the FPGA, however, according to the timing specifications in the sta sheet, the skew between DRY and DATA can be anywhere from +500 ps to -500ps. So, assuming the traces are all the same length, the setup time could be as low as -500ps and the hold time could be as low as -500 ps. How is this supposed to work? Is the only solution to delay the DRY using longer traces by1/2 clock cycle? Thanks and Best Regards,
-Tim Starr on behalf of MD@BD