This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7066: Why the first READ REGISTER (Opcode = \x08) after WRITE (Opcode = \x10) is not functioning, why is it functioning from the second READ (Opcode = \x10)??

Part Number: ADS7066


Tool/software:

Hello,
I am using ADS7066 as a SPI slave in single mode. Can you please help with the following question, suppose if I do below steps.
>> Sending bytes through SDI
>> Getting output from SDO
Steps:
1. I sent \x08\x04\x04 (3 bytes) to set the OP_MODE_CFG Register to Value 4.
2. Then, I send \x10\x04\x00 to read the register, I get random 3 bytes,  (First READ) = \x00\x0E\x00
3. Now, if I send \x10\x04\x00, I now get the read data which says \x04\x00\x00 (implies set)    (Second READ)
Question:
Why the first READ REGISTER after WRITE is not functioning, why is it functioning from the second READ??
//Snippet
write_to_spi_device(): Write_command: [<ADS7066_OpCode.WREG: 8>, <ADS7066_Register.OPMODE_CFG: 4>, <ADS7066_ClockDivider.CLK_DIV_4: 4>], read_result_values: {0: 2, 1: 0, 2: 0}  = \x02\x00\x00
read_from_spi_device(): Read_command: [<ADS7066_OpCode.RREG: 16>, <ADS7066_Register.OPMODE_CFG: 4>, <ADS7066_OpCode.NULL: 0>], read_result_values: {0: 0, 1: 14, 2: 0} = \x00\x0E\x00
read_from_spi_device(): Read_command: [<ADS7066_OpCode.RREG: 16>, <ADS7066_Register.OPMODE_CFG: 4>, <ADS7066_OpCode.NULL: 0>], read_result_values: {0: 4, 1: 0, 2: 0} = \x04\x00\x00
Note: I am using Ni8452 as a SPI master in the single mode with the below configurations to connect to SPI slave
// NI845x slave device connect configurations
        ni845x_spi.set_ni845x_spi_configurations(
            chip_select = dev_types.ni845x_types.ChipSelect.CHIP_SELECT_0,                       # Chip Select chosen for the SPI slave device
            sclk_rate = dev_types.ni845x_types.ClockRate.CLK_10000,                              # Deafult = 10MHz
            sclk_rate_polarity = dev_types.ni845x_types.Cpol.kNi845xSpiClockPolarityIdleLow,     # Default = LOW
            sclk_phase = dev_types.ni845x_types.Cpha.kNi845xSpiClockPhaseFirstEdge,              # DEFAULT = First Edge
            bits_per_sample = 8,                                                                   # ADS7066 sample size = 8bits
            port = 0                                                                                # Port 0 to 7 as 8 devices can be connected in Single Standard Mode
            )
Does sample size being set to 8 has anything to do with this behaviour from ADS7066??
Regards
Sai Satwik Vaddi
Developer
  • Hello Sai Satwik Vaddi,

     

    The ADS7066 requires 2 SPI frames to be able to read back from a register. the 1st SPI frame enables the readback and then the 2nd frame outputs the actual register value. This is why you aren't getting the value until your "2nd read". Please see Section 7.3.10.3.2 Register Read (below) for more information and a diagram. 

     

    Best regards, 

    Yolanda