Tool/software:
Hello Support team,
My customer observed UCOR=1 and COR=1 when reading 0x0F.
Could you please advise what causes this issue?
The following items are what I requested and got from the customer to help solve this issue.
=====
- The transient behavior at DACx outputs at power up as indicated in 9.4.2 At Power Up and Figure 50 in the datasheet is not observed.
- Reading 0x0F register is 0x06 (UCOR=1 and COR=1) right after power on. Then change the access level to Level 2, and write C32 to register 0x10 (software reset), the reading of 0x0F is 0x06. Because the Access level returned to Level 0, software reset seems to be effective.
- Communication between LMP92066 and the host is normal. The slave address set on LMP92066 and the setting at the host is the same. Other registers work normally. DAC output voltage can be changed arbitrarily.
- The circuit board is designed by the customer.
- The LMP92066 the customer is evaluating was purchased from some EC site such as Digi-Key.
=====
Could you please advise what issue could happen and what measures could be taken? Or is the LMP92066 the customer is evaluating abnormal?
Best Regards,
Katsuhiro