Tool/software:
Hello.
I would like to know about the functions of the DAC53202.
I am currently experiencing a problem with a product that uses the DAC53202.
It seems that noise is being mixed into the DAC53202's I2C signal, causing it to malfunction.
The malfunction is as follows:
During DAC output, OUT0 and OUT1 sometimes unintentionally go to high impedance.
When this state occurs, both OUT0 and OUT1 remain at high impedance even if the output setting is reset.
If the DAC53202's VDD is turned off and then turned on again, it will operate normally after that.
Is there a function that performs this kind of protection in the event of unauthorized communication, etc.?
If there is such a function, how can I disable the protection after it has operated?