Part Number: TX7316EVM
Tool/software:
Hello E2E Experts,
Good day.
I’ve been trying to drive TX7316EVM with GUI software, but it does not work well.
I used "Quick Setup” in 3-level mode. The 1-kHz sync signal was successfully observed. But 4-MHz or 5-MHz pulses were not observed.
I applied ±5 V and ±10 V to J3 and J1, respectively.
I checked trobleshootings described in the manual.
I could not understand reconfiguration of EVM to 3-level mode shown in Table 1.
Thus, I did not change anything on the board.
Is this a reason of the problem?
If so, do I have to buy extra components shown in “components to be added”?
Please let me know if the above solution is viable or problematic.
Regards,
CSC