Part Number: ADS122C04
Tool/software:
Hallo,
I have question regarding the "ADS122C04IPWR". In my project I am using "ADS122C04IPWR" with Renesas RX65N Microcontroller and communicating through I2C bus.
I am trying to read the Voltage on the inputs of ADS122 which will be converted to a digital value. However, I always ended up getting the half value of the inputs, please find below the configuration details:
CONF_REG_0_AIN0 0x81 // setting AINP = AIN0, AINN = AVSS, Gain = 1 (default), PGA disabled and bypassed
CONF_REG_0_AIN1 0x91 // setting AINP = AIN1, AINN = AVSS, Gain = 1 (default), PGA disabled and bypassed
CONF_REG_1 0xC4 // 1000 SPS, Normal mode, Analog supply (AVDD – AVSS) used as reference and even I tried 0xC0 which will uses Internal 2.048-V reference
CONF_REG_2 0x00
CONF_REG_3 0x00
I2C-Bus:
I2C transfer rate 400Kbps
Operating frequency PCLK 60 MHz
At this moment I have cut-off my circuit and provided a direct voltage on the ADS "AIN0 and AIN1" through a power supply, also getting the half values. As I mentioned before I also tried to change the reference voltage
from my (AVDD = 4.6 to the internal = 2.048) in both cases I get the half value. I have also checked the GND of my board, some where I read if there are two separated GND, could makes an issue.
Last, in data sheet part "8.3.9 System Monitor" says i can measure analog power supply using the internal 2.048-V reference, unfortunately I got also the half value.

Know I am out of solutions and I need your kind support to solve this issue.
Best Regards
Ibrahim