Tool/software:
Hi team,
My customer is using DAC38J84 QMC function. They configure the register like below. When set the config16(qmc_phaseab) to 0x7ff or 0x800, the QMC don't work, and the IQ waveform is abnormal. Could you please help to elaborate how to configure to QMC and check why the waveform is abnormal?
register configuration:
Config0: Enable bit 12/13
Config16:
0x000: yellow=I blue=Q 132mV

0x7ff (“011111111111” = 0.49975.) Abnormal: the I signal is distortion.

0x800: (“100000000000” = –0.5.) Abnormal: the I signal is decrease to half.

BRs,
Rannie