Part Number: AFE5816
Tool/software:
Hi, everyone
Now i'm trying to test output of the AFE5816.
This is my register setting sequence for low-power mode operting.
01h / 0014h
41h / 8000h
42h / 8000h
41h / 0000h
42h / 0000h
03h / 2000h
04h / 0001h
00h / 0010h (for DTGC mode)
b6h / 8820h
b5h / 00c0h
Additionaly, my adc_clk has 20MHz frequency.
Case 1) Test pattern output
When i write 02h / 0080h for testing and measuring DOUTN pin, then result is like the figure below

output is same with desired one.
But, when i try to test with arbitary sine waveform generated by function generator, there are no output signals..
I made 1MHz frequency, 400mVpp amplide, No offset value sine waveform. And this is waveform measured at INP pin.

When i measure DOUTN pin with this sine waveform input, there are no output signal but only noise signal (very low amplitude compared to test pattern output) that have frequency same with fclk like the figure below

Is there any problem with my register setting? or is there anything I can test to deal with this problems?
Additionaly, if there are no input to AFE5816 device, then DOUTN pin always have '1' value?
Thank you.